- Getting started
- Creating projects
- OPC UA
- Graphic objects
- Predefined graphic objects
- Sessions and locales
- Object and variable references
- Extending projects
- NetLogic
- NetLogic tutorial
Configure the trusted server certificates at design time
Set the server certificate rejected when importing nodes with an OPC UA client object as trusted to be able to import these nodes at design time.
You can move the certificate in the following ways:
- Manually, by using Windows Explorer on a Windows target only.
- Remotely, by usingFactoryTalk Remote Access.
- By using the same application.
- FromApplicationFiles/PKI/Rejected, move the certificate toProjectFiles/PKI/Trusted/Certs.
Provide Feedback