- Getting started
- Creating projects
- OPC UA
- Graphic objects
- Predefined graphic objects
- Sessions and locales
- Object and variable references
- Extending projects
- NetLogic
- NetLogic tutorial
Import nodes from NodeSet
Import all nodes from a NodeSet
XML
file.
TIP:
Import nodes from NodeSet to import all nodes from
OPC UA Companion Specifications
defined in a NodeSet file. For more information, see OPC UA Companion Specifications.Prerequisites
Obtain an
XML
file with NodeSet to import.- To import nodes from NodeSet
- InProject view, right-clickModelfolder or any of its subfolders and then select .
- Select theXMLwith NodeSet to import.
The imported nodes appear in the folder.
Provide Feedback