- Getting started
- Creating projects
- OPC UA
- Graphic objects
- Predefined graphic objects
- Sessions and locales
- Object and variable references
- Extending projects
- NetLogic
- NetLogic tutorial
Create an enumeration
Create an enumeration object and define enumeration members in the editor.
- Right-click a node to contain the enumeration and select.
- SelectEnumerationand chooseSelect.Enumerationappears under the node.#
- InProject view, double-clickEnumeration.#Enumeration editor displays in the central pane.
- In the editor, manage the enumeration members:
- To add a member, selectand complete:
- Value. Enumeration member value. Value is generally a consecutive integer.
- Display name. Name of the enumeration member.
- Description. Additional information about the enumeration member.
- To edit aValue,Display name, orDescription, double-click the corresponding cell and enter a new value.
- To remove a member, select a cell in the corresponding row and select.Delete
Provide Feedback