Create an object

Create an object

Create an object to add a node to the project.
  1. In
    Project view
    , select the folder in which to create the object and then select
    Add
    in the
    Project view
    toolbar.
    TIP: You can also right-click a folder in
    Project view
    and use the
    New
    context menu to create objects.
    The context menu displays objects that the folder can contain based on the folder category.
  2. Select the object to add to the project.
The new object appears in
Project view
.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.