Open an object
Open an object from
Project view
.- InProject view, double-click the object or mouse over the object and then select.
The object opens in a separate tab if the object has a dedicated editor.
Properties
for the object also open.Provide Feedback