Array editor
Use the array editor to modify the values of array variables.
Array editor

Item | Name | Description |
---|---|---|
![]() | ![]() Add | Adds a cell to an unconstrained array. |
![]() | Delete | Removes a cell from an unconstrained array. |
![]() | Array cells column | Lists array cells. |
![]() | Array values column | Lists editable array cell values.
TIP:
If the array lists colors, you can select the color preview to open the color selector.
|
![]() | Apply button | Applies changes to the array values and closes the editor. |
![]() | Cancel button | Cancels changes to the array values and closes the editor. |
![]() | Open in tab button | Opens the array editor in the central pane. |
Provide Feedback