- Getting started
- Creating projects
- OPC UA
- Graphic objects
- Predefined graphic objects
- Sessions and locales
- Object and variable references
- Extending projects
- NetLogic
- NetLogic tutorial
Create a project
A project contains elements with which a
FactoryTalk Optix Application
is made. You can create either a local project or a project from a remote location.- In the main toolbar, select.ProjectThe Start page opens.
- SelectNew.
- To create a local project that has a default window and configured categories inProject view, select the project type: .
- Default. Create a project with all categories and a main window inProject view.
- OptixPanel. Create a project with all categories and a main window inProject view, in addition to:
- ASystemobject with a pre-configuredFT Remote Accesswidget to request access to the FactoryTalk Remote Access server and assistance from the FactoryTalk Remote Access application.
- ASettingsWidgetsfolder that containsNetwork Settings,Device Settings,Date & Time, andLoad Applicationwidgets.
- A main window that displays and allows you to navigate the default widgets at runtime as well as place your own content on the Home page of the window.
- Automatic language switching for widgets.
- An enabled virtual keyboard
To create a blank project that has no default content, inFactoryTalk Optix Studio Options, selectAdvanced modeand then restartFactoryTalk Optix Studioto selectBlankon the Start page. See Set options. - InName, type the name of the project.
- InLocation, type the path to the project.The default location is. SelectC:\Users\UserName\Documents\Rockwell Automation\FactoryTalk Optixto browse for a different location.Browse files
- (optional) SelectUse version control.With version control enabled, you can back up the state of your project to a local repository and push local changes to a remote repository.
- (optional) SelectEncrypt secretsto encrypt project passwords, custom objects that have thePasswordDataType, andYAMLfiles that represent the project information model.To enable theEncrypt secretsoption, log in toFactoryTalk Hub. For more information, see Project secrets encryption.
- UnderSet main window size, specify the width and height of the main window when you create projects. Accept the defaultCustomwindow size, enter a newWidthandHeightfor a new custom window size, or select a pre-configured window size or OptixPanel if you are creating an OptixPanel project.The default custom window size is 400 x 400 pixels.
- SelectCreate.
- (optional) To create a project from a remote location:
- SelectRemote.
- InRemote URL, enter the URL of your remote repository supplied by your System Administrator to specify the remote project that you want to open.
- InLocation, enter the folder on your local computer where you will save and commit changes before pushing them to the remote repository.
- SelectOpen.If you are signed in toFactoryTalk Optix, you do not have to know theRemote URLorLocation.Create a new projectautomatically displays all of the potential repositories accessible with your GitHub account and all of the remote projects that you can open.Opening project from remoteappears in the status bar and the new project opens with the same name as the remote repository.
The new project opens. If there was an existing project open, the project opens in a new instance of
FactoryTalk Optix
.Provide Feedback