Duplicate a recipe schema
Duplicate a recipe schema based on the existing recipe schema.
- From the toolbar, select.Open dashboard page
- In the central pane, selectConfigure a recipe.
- Right-click the available recipe schema and selectDuplicate.
If necessary, edit the duplicated recipe schema. See Edit a recipe schema.
Provide Feedback