Manage recipes at runtime
Use the recipes editor widget to store a new recipe, to delete an existing recipe, or to apply a recipe on the controller.
Prerequisites
- To manage recipes at runtime
- To store a new recipe:
- Edit the values of the ingredients.
- In the recipe list, enter a name for the recipe.
- SelectSave.
- To delete a recipe, select a recipe and selectDelete.
- To apply a recipe on the controller:
- Select a recipe.Recipe ingredients values display.
- SelectApply.In the right column, ingredients values loaded to the controller display.
- To change the values of the ingredients on the controller, edit the values, selectSaveand selectApply.The values of the ingredients on the controller update in the right column.
Provide Feedback