Recipes editor
The recipes editor widget contains the graphical objects and NetLogic scripts required to display and manage the recipes at runtime.
Use the recipes editor widget to:
- Display ingredients and values of a stored recipe during editing or loading the controller
- Create, edit, or delete a recipe
- Store a recipe in the database
- Load a recipe from theFactoryTalk Optix Applicationto the controller
- Load a recipe from the controller to theFactoryTalk Optix Application
Recipes editor interface
Recipes editor example

Item | Name | Description |
---|---|---|
![]() | Recipe name | Assign a name to a new recipe or select an existing recipe. |
![]() | Recipe control buttons |
|
![]() | Ingredients list | Recipe schema ingredients. |
![]() | Ingredient values editor | Editable values of the recipe ingredients. |
![]() | Applied ingredient values | Values of the ingredients on the controller. |
Provide Feedback