Time zones in trend graphs

Time zones in trend graphs

At runtime, the
Trend Graphic
object displays data in the X-axis in the UTC standard time zone.
Use the
Reference time zone
property of the graph to specify whether data display in the local time zone or the session time zone. When the
Trend Graph
object is connected to a
Data logger
, you must enable the
Local time log
property of the application to store data in the local time zone.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.