Configure the authentication mode
Change the default authentication mode to allow local users and domain users to log on at runtime.
Prerequisites
To allow Active Directory users to authenticate, either:
- Obtain the Active Directory domain name and server address.
- Ensure that theWindowsclient is joined to the Active Directory domain.
To allow LDAP users to authenticate, obtain:
- LDAP server address
- CA certificate file
- To configure the authentication mode
- InProject view, select the root node.
- InProperties, expandAuthentication, and then inAuthentication mode, select the authentication type that allows specific users to log on:
- Model only. Users created inFactoryTalk Optix Studio.
- Local only. Local machine users.
- Domain only. Active Directory and LDAP users.
- Domain and local. Active Directory, LDAP, and local machine users.
- Any. Users of any type.
- (optional) SetDefaultUserFolderto change the default folder to contain user objects.TIP: The default folder to contain user objects is. When a domain user logs in at runtime, a corresponding user object appears in the folder specified.
- (Domain only) InDefault domain name, enter the default domain name for domain users that log on at runtime.TIP: If you leave Default domain name blank, the domain name is set based on the Active Directory domain joined by theWindowsclient or retrieved from the LDAP server.
- ( Doma in only) InDefault server address, enter the Active Directory or LDAP server address.TIP: If you leave Default server address blank, the Active Directory server address is set based on the Active Directory domain joined by theWindowsclient.TIP: If you do not specify the port in the server address, the default 389 port is used.
- (LDAP only) InCA certificate file, selectBrowseand select the certificate file.TIP:To find items, start typing the item name to find inSelect file.If the file does not appear inSelect file, selectand inImport file(s)Import file(s), select the file to import and then chooseSelect.TIP: If you leave CA certificate file blank, the localWindowsmachine is used to authenticate the user. CA certificate file is required to authenticate against a specific LDAP server or use a Linux client.
Provide Feedback