Create a group
Groups are recommended for determining the rights and privileges assigned to users.
For example, a user who is part of an administrator group has administrative rights.
- InProject view, expandSecurity.
- Right-clickGroupsand select .
- (optional) To create subsequent groups, right-clickGroupsand then select .New groups appear in bothProject viewand inManage Users and Groups.
- (optional) To rename a group, right-click the group, selectRename, and then enter a new name for the group.
- Select.Save
Provide Feedback