Change user properties

Change user properties

Change the properties of a user to modify the domain, password, location, and language for that user.
  1. In
    Project view
    , expand
    Security
    .
  2. Expand
    Users
    .
  3. Select a user.
  4. In
    Properties
    , change:
    • Name
      . Name of the user.
    • Password
      . Password that the user must provide to log on to the application.
    • LocaleIds
      . Location of the user. The default is en-US.
    • Languages
      . Language configured for the user. The default language is the default language of the location of the user. 
    • Measurement system
      . The measurement system used to display data to the user:
      • International system of units
      • US customary measurement system
      • British imperial units
    • Domain
      . Identifies the local
      Windows®
      user account for a domain-linked user account.
  5. Select
    Save
    .
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.