Create a remote repository for a project

Create a remote repository for a project

Create a remote repository to enable multi-user collaboration on a project.
  1. Create a blank remote repository with tools supplied by the supported version control provider.
    IMPORTANT: The remote repository cannot contain any files, including the
    README
    ,
    .gitignore
    , and
    LICENSE
    files.
  2. Create an initial project named the same as the repository. See Create a project from a remote repository.
    IMPORTANT: The project and repository names must match, including capitalization.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.