Session activity log and audit
The C# APIs are supplied by the
Session
C# class and displayed by NetLogic, which represents the session in which the instance of NetLogic at runtime exists.Provide Feedback