Asynchronous task

Asynchronous task

Create asynchronous tasks to run code asynchronously.
TIP:
FactoryTalk Optix Studio
provides C# class specifications that exhibit the constructors that you can use for creating asynchronous tasks. The constructors are based on the .NET Framework C#
System.Threading.Tasks.Task
class, which represents an asynchronous task. See Task Class.

Available classes

You can use these classes to create asynchronous tasks:
PeriodicTask
A task that runs code at regular time intervals.
DelayedTask
A task that runs code after a time delay.
LongRunningTask
A task that requires significant time or CPU resources.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.