Prepare the remote machine for debugging

Prepare the remote machine for debugging

Install and configure the Remote Debugger desktop application.
Prerequisites
Download and install Visual Studio Debug Tools from Remote Debug a C# or VB project - Visual Studio (Windows) | Microsoft Docs.
  1. To prepare the remote debugging target machine
  2. Open the Remote Debugger desktop application.
  3. Observe the device and port  to connect to the remote debugging target.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.