- Getting started
- Creating projects
- OPC UA
- Graphic objects
- Predefined graphic objects
- Sessions and locales
- Object and variable references
- Extending projects
- NetLogic
- NetLogic tutorial
Integrate the interface with the NetLogic
Make the button trigger the label text change when you select the button.
- InProject view, selectButton1.
- InEvents, next toMouseClickEvent, selectand select .
- Create a dynamic link betweenlabelNodeIdandLabel1.For more information about dynamic links, see Create dynamic links.
Provide Feedback