- Getting started
- Creating projects
- OPC UA
- Graphic objects
- Predefined graphic objects
- Sessions and locales
- Object and variable references
- Extending projects
- NetLogic
- NetLogic tutorial
Add the Zip Unzip NetLogic
The Zip Unzip NetLogic enables you to compress and decompress files and folders.
Prerequisites
Set the default external code editor. See Set the default code editor.
- To add the Zip Unzip NetLogic
- From the toolbar, select.Template Libraries
- InLibraries, from the top list, selectScripts.
- From theComponentslist, dragZip Unziponto theMainWindow (type)inProject view.
- SelectClose.
- Add the NuGet Gallery | SharpZipLib package. See Add NuGet packages.
The Zip Unzip NetLogic is added to your project. The NetLogic exposes the
CreateZipArchive
and UnzipArchive
methods. For reference, see ZipUnzip NetLogic.Provide Feedback