Terms dictionary
Terms related with
FactoryTalk Optix
.- argument
- Input and output parameters of a method.
- DBMS
- Database management system.
- headless device
- Device without display. For example, a web server or an IoT device.
- DSN
- Data source name, which contains information that enables an application to connect to a database with a driver.
- event
- Methods and commands defined at design time to be executed if certain conditions are met during runtime.
- locale ID
- A label (for example,en-US) composed of two segments (for example,enandUS). The first segment identifies the language and country of the user interface. The second segment defines the measurement units and date and time format.
- instance
- An object or variable derived from an object type or variable type.
- locale
- The country and language settings of a given user, represented by alocale IDlabel.
- application logic
- Programming logic that determines the application behavior at runtime.
- method
- An action exposed by an object and or a NetLogic that is executable at design time or at runtime. When invoked, it runs a set of instructions.
- information model
- Nodes that describe the structure and characteristics of a project node or entire project.
- interactive session
- A session generated at runtime by a Presentation Engine if the application has a graphical interface.
- node
- An elemental unit in an information model.A node can be:
- An object type
- A variable type
- A variable
- A method
- ODBC
- Open Database Connectivity API for accessing database management systems.
- object
- A node that can contain objects and variables that represent either:
- Physical objects. For example, a motor.
- Abstract objects or features. For example, a recipe.
- OPC UA
- Open Platform Communication Unified Architecture, a smart manufacturing standard of machine-to-machine communication.
- predefined type
- Type of object or type of variable included by default in the development environment.
- Presentation Engine
- An object that creates an interactive session to display the UI at runtime.
- property
- Indivisible variable of a node. In the context of C#, an inseparable element of a class.
- FactoryTalk Optix Application or FTOptixApplication
- An HMI or Internet of Things application generated byFactoryTalk Optix Studiothat runs on a target system.
- FactoryTalk Optix Studio
- FactoryTalk® Optix Studio™integrated development environment (IDE) for designing and deploying HMI and Internet of Things applications.
- session
- A runtime context of aFactoryTalk Optix Applicationin which a user runs read and write operations based on their permissions.
- structured variable
- A variable that contains other variables, for example an analog variable.
- tag
- A Controller variable.
- target
- Systems or devices on which you can run aFactoryTalk Optix Application. For example, an HMI panel, a web server, or an Internet of Things device.
- type
- A model of an object or variable from which object instances or variable instances are derived.
- URI
- A uniform resource identifier, a sequence of characters that uniquely identifies a resource.
- Resource URI
- Represents the path (URI - Uniform Resource Identifier) of a file or a resource inside or outside the project.
- UUID
- A universally unique identifier.
- variable
- A Node that represents the value of a figure, which can contain other variables.
- widget
- A reusable graphical object, which can contain other objects and variables. For example, a panel for configuring users.
Provide Feedback