FactoryTalk Optix Studio

FactoryTalk Optix Studio

FactoryTalk Optix Studio is an integrated development environment with a framework of functional modules for designing and compiling HMI or Internet of Things (IoT) applications.
FactoryTalk Optix Studio
includes a library of predefined objects that support the modular design of graphical interfaces, features, and logic operations of an HMI application. By using specific C# language scripts, you can automate various actions in the design phase and add customized functions to projects.

Desktop and web editors

FactoryTalk Optix Studio
is available as a web and a desktop development environment that you use to build
FactoryTalk Optix Applications
  and deploy them to client systems. You access
FactoryTalk Optix Studio web editor
through
FactoryTalk Hub
.
If there is an Internet connection outage,
FactoryTalk Optix Studio web editor
tries to reconnect to the Internet every 5 seconds. During that period, you cannot interact with
FactoryTalk Optix Studio web editor
. Once
FactoryTalk Optix Studio web editor
reconnects to the Internet, you can continue where you left off.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.