FactoryTalk Optix Studio web editor
You can use
FactoryTalk Optix Studio
in a web browser through FactoryTalk Hub
.Editor features support
FactoryTalk Optix Studio web editor
supports all FactoryTalk Optix Studio desktop editor
features except for:
- Save logs from theOutputtabs.
- Edit NetLogic files.
- OpenFactoryTalk OptixHelp.
- Display paths in logs in theOutputtabs.
- Add files and images by dragging and dropping them intoFactoryTalk Optix Studio web editor.
- Restart the application at runtime by using themethod.
Emulator features support
FactoryTalk Optix Studio web editor
emulator supports all features of FactoryTalk Optix Studio desktop editor
emulator except for:
- Control theWebBrowserobject in the runtime emulator.
- Control thePDFViewerobject in the runtime emulator.
- Control theVideoobject in the runtime emulator.
- Control theWindowobject in the runtime emulator.
Provide Feedback