Corrected anomalies in this release

Corrected anomalies in this release

The list identifies the anomalies corrected in
FactoryTalk Optix
1.2.0.
Use the identification information in parenthesis to track the anomaly in future releases or for reference when receiving assistance from Customer Support with a related issue.
Error opening project located on OneDrive [1911544]
When a project is located on OneDrive, pulling an update from the remote repository may result in an error when the project is opening. Restart
FactoryTalk Optix Studio
and reopen the project.
This anomaly first identified in version 1.0.2.
Unable to connect to Logix controllers from the Emulator using FactoryTalk Optix Studio in the web version [1900931]
Unable to read and write to logic controllers when emulating a project using the
FactoryTalk Optix Studio web editor
. Use the
FactoryTalk Optix Studio desktop editor
to emulate projects that reference Logic controllers.
This anomaly first identified in version 1.0.2.
Online import of UDTs may be incorrect if the UDT type and a Logix data type have the same name [2131416]
When performing an online tag import, if the name of a UDT type became a predefined type in a later version of Logix, the UDT will not import correctly. For example, if you create a UDT in Logix version 32 and name the UDT Time, an online import will create the tag of type Time as defined in Logix version 34 instead of how the UDT was defined in Logix version 32. To resolve this issue, either perform an offline import or change the name of the Logix UDT type.
This anomaly first identified in version 1.1.0
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.