Confirm and acknowledge alarms

Confirm and acknowledge alarms

Acknowledge and confirm active alarms at runtime. Acknowledging an alarm indicates that the user is aware of the alarm. Confirming an alarm indicates that the cause of the alarm is resolved.
  1. At runtime, in the
    Alarm grid
    , either:
    • Select an alarm. Any interaction applies to only the selected alarm in the grid.
    • Select no alarm. Any interaction applies to all of the alarms in the grid.
  2. Select either:
    • Acknowledge
      or
      Acknowledge all
      . Acknowledge that you are aware of the selected alarm or all alarms.
    • Confirm
      or
      Confirm all
      . Confirm that the origin of the selected alarm or all alarms have been resolved.
Checkmark
appears in the related column of the alarm.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal