Configure a Histogram chart

Configure a Histogram chart

Configure a
Histogram chart
object to get data from a project node or a database.
  1. In
    Project view
    , in
    UI
    , right-click a container and then select
    New
    Data controls
    Histogram chart
    .
  2. In
    Properties
    , create a dynamic link between the
    Model
    property and a node.
    Selected node
    Combo box
    Database object
    Values contained in database tables.
    Project node
    Values of attributes or properties of all direct child nodes.
    For more information about dynamic links, see Create dynamic links.
  3. (optional) Specify the kind of items to display in the object by setting
    ItemKind
    .
    TIP:
    The
    ItemKind
    property is automatically set with the object or variable type recognized among the child nodes.
    For example, if the model is based on a folder node that contains several instances of a
    Motor
    object type,
    ItemKind
    is automatically set with the reference to the type. In this case, the values that display are the attributes or properties of different instances (, , , and so on).
  4. Configure chart labels by creating a dynamic link between
    Label
    and a variable argument such as, .
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.