Display information model graphs

Display information model graphs

Visualize information models of
FactoryTalk Optix
projects in the form of graphs.
TIP: For more information about project information models, see Information model.
Prerequisites
Install an application that displays graphs
DGML
graphs, such as Microsoft Visual Studio with the DGML Editor component.
  1. To display information model graphs
  2. Do either:
    • In
      Properties
      , right-click the property.
    • In
      Project view
      , right-click the project node.
  3. Select
    Model analysis
    and then select either:
    • Information model graph (Project only)
      . Visualize only nodes, types, and references related to the user project.
    • Information model graph (Ignore OPCUA/Core namespaces)
      . Visualize nodes, types, and references of the user project and
      FTOptix
      modules namespaces, except OPC-UA and Core namespace.
    • Information model graph
      . Visualize all nodes, types, and references of any namespace.
Information model graph example
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal