Create a node pointer

Create a node pointer in
Project view
to reference to another node of the project.
  1. In
    Project view
    , select the folder or object to contain the variable.
  2. In
    Properties
    , create a dynamic link to the node to point to.
    For more information about dynamic links, see Create dynamic links.
  3. (optional) expand
    NodePointer
    #
    and complete these properties:
    • Kind
      . The kind of the node that the node pointer targets.
    • Node class
      . Either:
      • Instance
      • Type
      • Any
  4. (optional) In
    Properties
    , select
    Add
    , select
    Display name
    , and enter the display name.
  5. (optional) In
    Properties
    , select
    Add
    , select
    Description
    , and enter the description.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal