Project backup

Project backup

FactoryTalk Optix Studio
automatically creates backups of projects.
Projects are automatically backed up when:
  • You save a project
  • You update a project to a more recent version of
    FactoryTalk Optix Studio
  • You restore a project from backup. See Restore a project.
The default location for the backup folder is:
%localappdata%\Rockwell Automation\FactoryTalk Optix\Studio\Backups\
Project Name
Each of the project folders consists of other subfolders with the following types of backups:
  • Automatic
    . Three backups, performed when saving the project.
  • Recovery
    . One backup, performed when a corrupt project is opened and repair attempted. See Restore a project.
  • Upgrade
    . Two backups, performed when updating the project to a more recent version of
    FactoryTalk Optix Studio
    .
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal