Close a project

Close a project

Close a project from the Start page.
You can have more than one project open at a time. When you open additional projects, additional instances of
FactoryTalk Optix Studio
open.
  • From the main toolbar, select
    Project
    . On the Start page, select
    Close
    .
    TIP: If you open the Start page from an open project and want to close the Start page, select .
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal