Export a FactoryTalk Optix Application

Export a FactoryTalk Optix Application

Export a
FactoryTalk Optix Application
to deploy the application to client devices that are not accessible in the network.
  1. Select the arrow next to
    Save
    to open the drop-down menu and then select
    Export
    FactoryTalk Optix Application
    .
  2. In the dialog, complete:
    • Platform
      . Select the operating system of the client device.
    • Location
      . Type the path to the location where you want to save the
      FactoryTalk Optix Application
      . Alternatively, select the folder icon to browse to the folder.
      TIP: A folder can only contain one
      FactoryTalk Optix Application
      . Each
      FactoryTalk Optix Application
      must use a separate folder.
  3. (optional) If available, fill
    Password
    to password-protect the exported application.
    The exported application is encrypted. You will be prompted to enter the password when importing the application to the client device.
  4. Select
    Export
    .
A progress window displays while the
FactoryTalk Optix Application
is being exported. After the export has completed, a dialog appears to inform you that the
FactoryTalk Optix Application
was successfully exported to the location specified.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal