Remove a client device

Remove a client device

Remove client devices that you no longer need.
  1. From the main toolbar, next to
    Run
    , select the client dropdown menu.
  2. (optional) In
    Client device settings
    , to display only the active remote client devices, toggle
    Active remote devices
    .
    TIP: Refresh remote client devices by selecting
    Refresh
    .
  3. Select a client device.
  4. Select
    Remove the selected target device
    .
  5. In the
    Client device settings
    , select
    Remove
    .
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal