- Getting started
- Creating projects
- OPC UA
- Graphic objects
- Predefined graphic objects
- Sessions and locales
- Object and variable references
- Extending projects
- NetLogic
Develop an archives manager
Use the preconfigured Zip Unzip NetLogic to create, extract, and password-protect ZIP archives.
Example application

TIP:
You can download a sample project from:
ArchivesManager.zipPrerequisites
Select
to run the project using the client emulator to test your project. To run the project on a remote client, see Add a client device.
Run
Provide Feedback