Variables

Variables

A variable is an element that represents a figure or a characteristic of an object and specifies the value of that characteristic.

Variable overview

Each variable:
  • Contains a DataType attribute
  • Can be structured to contain other variables
  • Contains descriptive attributes
  • Cannot contain objects
TIP: You cannot remove properties from predefined objects. For example, you cannot remove the
Text
property from a
Label
object.

Variable examples

For example, a variable can represent:
The speed of a physical object
The
Speed
variable with a numeric (Int32) value defines the speed of the Motor object.
A style characteristic of a graphic object
The
Text color
variable defines the color of the Label object
Various object properties
A dynamic link to the
EmbeddedDatabase1
object defines the Store variable value.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal