Configure a digital alarm

Configure a digital alarm

Configure a simple Boolean alarm that warns you about issues with Motor1 at runtime.
TIP: By default, a digital alarm triggers when its
Input variable
equals to 1. For more information, see Alarm types.
  1. In
    Project view
    , right-click
    Alarms
    and select
    New
    Digital alarm
    .
  2. In
    Properties
    , create a dynamic link between the
    Input variable
    and
    Motor1Alarm
    variable.
    For more information about dynamic links, see Create dynamic links.
  3. In
    Message
    , enter a warning message.
    For example, enter
    Motor1 alarm
    .
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal