- Getting started
- Creating projects
- OPC UA
- Graphic objects
- Predefined graphic objects
- Sessions and locales
- Object and variable references
- Extending projects
- NetLogic
Corrected anomalies in this release
The list identifies the anomalies corrected in
FactoryTalk Optix
1.3.0.- Clearing option buttons triggers Modified value event [2161125]
- The Modified value event of an option button triggers when you select or clear the option button. TheCheckedproperty changes toTrueorFalse. For example, selecting another option button in a group triggers the Modified value event of the cleared option button.In version 1.3.0, manually selecting an option button triggers the Modified value event for the selected option button. If manually selecting an option button clears another option button in a group, the Modified value event does not trigger for the cleared option button.This anomaly corrected in version 1.3.0.This anomaly first identified in version 1.0.3.
- Loading application from USB may result in multiple applications [2238992]
- Loading an application to a device from a USB results in multiple applications on the device if the exported application is not encrypted.This anomaly corrected in version 1.3.0.This anomaly first identified in version 1.2.0.
- Embedded Edge Compute module does not support NativePresentation Engine [2233502]
- If an application deploys with the NativePresentation Engine, the library cannot load and the application does not run on the device. Replace the NativePresentation engine with a WebPresentation engine to allow a remote client to connect to the device.This anomaly corrected in version 1.3.0.This anomaly first identified in version 1.2.0.
- Embedded Edge Compute module AOP Electronic keying may result in an unexpected error or connection in Logix [2256502]
- Embedded Edge Compute module AOP Electronic keying may result in an unexpected error or connection in Logix for a minor revision mismatch. Update the AOP Definition to disable keying for the module.This anomaly corrected in version 1.3.0.This anomaly first identified in version 1.2.0
- Tag import for offline project displays .ACD file error [2324005]
- Importing tags into an offline project that contains a communication driver displays the message "Failed to import tags: Invalid ACD file" when you use the tag importer and browse for the .ACD file. Save the .ACD file and then double-clickTagImporterto import the tags successfully.This anomaly corrected in version 1.3.0.This anomaly first identified in version 1.2.0.
- Media controls cause memory leaks on some devices [2183160]
- Excessive screen switching to screens that contain PDF and Video controls causes memory leaks on OptixPanels and Embedded Edge Compute devices.This anomaly corrected in version 1.3.0.This anomaly first identified in version 1.2.0.
- Application may not load on deviceafter deleting previous application[2248640]
- The default application may not load on the device after deleting an application using Device Manager. A deployed application may also display a blank screen after the deletion. To load an application on the device again, reboot the device.This anomaly corrected in version 1.3.0.This anomaly first identified in version 1.2.0.
Provide Feedback