- Getting started
- Creating projects
- OPC UA
- Graphic objects
- Predefined graphic objects
- Sessions and locales
- Object and variable references
- Extending projects
- NetLogic
Known anomalies in this release
The list identifies the known anomalies in
FactoryTalk Optix
version 1.3.0.Use the identification information in parenthesis to track the anomaly in future releases or for reference when receiving assistance from Customer Support with a related issue.
- DNS names in certificate must be lowercase [2226560]
- DNS names used in theSubjectAltNamefield of the certificate configuration are only recognized if they are lower case.This anomaly first identified in version 1.2.0.
- Special characters not always supported [2123530]
- Special characters are not supported in PDF filenames, FTP Server usernames, Git repository names, ODBC database names, or when using the Microsoft Pinyin input method on the device or at design time in FactoryTalk Optix Studio web editor.This anomaly first identified in version 1.2.0.
- Unable to deploy to device with invalid name [2239099]
- Deploying to a device with a name that contains a slash results in an error or the application not running on the device.This anomaly first identified in version 1.2.0.
- Versioning may result in an Object Type duplication or loss during a pull operation [2243507]
- Pulling from the remote repository when an Object Type name has been modified both remotely and locally causes a merge conflict. The operation creates two different objects when keeping local changes and causes the loss of the renamed type when accepting remote changes. To avoid data loss, all users collaborating on the project must manually update the Object Type name on their local project before pulling from the remote repository.This anomaly first identified in version 1.2.0.
- Compute Module with multiple backplanes in controller path unable to communicate with controller
- The Compute Module cannot communicate with the controller if there is more than one Backplane in the controller path. For example, the module is unable to communicate with the controller if the path is Backplane\1\A\10.220.173.66\Backplane\3. However, paths resembling either Backplane\3 or Backplane\1\A\10.220.173.66 allow the module to communicate with the controller.This anomaly first identified in version 1.2.0.
- FactoryTalk Optix delays opening when version control providers are unavailable [2357834]
- If the version control provider identity does not have network access to the on premises server, FactoryTalk Optix delays opening. For each version control provider identity that is unavailable, a 25 second delay occurs when opening FactoryTalk Optix.This anomaly first identified in version 1.3.0.
- Image does not appear at runtime [3140280]
- If an image file in a project does not appear in the runtime application, use a third party application to resize the image and make it smaller.This anomaly first identified in version 1.3.0.
- Unable to export file when name of project contains special characters [3110366]
- Filenames cannot contain special characters.This anomaly first identified in version 1.3.0
- No error appears when misconfiguring a string as a Discrete Input for a Modbus Station and all other tag reads fail [2351429]
- Assigning a string tag to a Discrete input memory area does not display an error message and causes read errors on all tags for the Modbus Station containing the misconfigured tag.This anomaly first identified in version 1.3.0.
- Renaming a user-defined library using OneDrive may result in synchronization errors [2348900]
- OneDrive is not recommended for storing user-defined libraries and may result in synchronization errors and duplicate files when renaming libraries. If attempting to use OneDrive to rename a library, unlink OneDrive when renaming the library. To unlink OneDrive, see Turn off, disable, or uninstall OneDrive.This anomaly first identified in version 1.3.0.
- Sparkline range cannot display if only one range is modified [3153055]
- If you modify only the value for Range high or Range low for a sparkline, the range cannot display in sparkline. Modify both the value in Range high and Range low to display the range in the sparkline.This anomaly first identified in version 1.3.0.
- Custom library elements do not appear without restarting FactoryTalk Optix [2371413]
- Elements added to a custom library do not appear inLibrariessearch until you restart FactoryTalk Optix.This anomaly first identified in version 1.3.0.
- Some videos may not play on computers running Microsoft Windows [2212837]
- If you emulate a project on a computer that is runningMicrosoft®Windows®, some videos may not play. Videos will play if you deploy the project to a device.This anomaly first identified in version 1.1.0.
- Unable to emulate a project [3196019]
- The Emulator cannot run a project that contains a Rockwell Automation EtherNet/IP station if FactoryTalk Optix Studio is installed in a folder that contains a special character.This anomaly first identified in version 1.3.0.
- Unable to launch FTOptixRuntime.exe [3187395]
- FTOptixRuntime.exe cannot launch if you export the project to a folder with a name that contains a special character.This anomaly first identified in version 1.3.0.
Provide Feedback