- Getting started
- Creating projects
- OPC UA
- Graphic objects
- Predefined graphic objects
- Sessions and locales
- Object and variable references
- Extending projects
- NetLogic
View alarms in UTC time zone
Alias the
Time
property of the Alarm grid
object to view events in the UTC (Coordinated Universal Time) time zone standard. UTC is the time standard on which all time zones are based worldwide. Viewing alarms in the UTC time zone ensures that all users are seeing the same time stamps for the alarms. - In the main toolbar, select.Template Libraries
- InTemplate Libraries, selectWidgets.
- Drag theAlarms Gridobject to the desired folder in theUIfolder.AlarmGrid# (type)appears.
- InTemplate Libraries, selectClose.
- In the editor, select the alarm grid and then inProperties:
- ExpandTimestamp.
- Expand theData gridcategory.
- Expand theColumncategory and then selectDataItemTemplate.
- InText, select.Add Dynamic Link
- In theDynamic Linkswindow, expandAliases.
- ExpandAlarm Conditionand then selectTime.
- ChooseSelect.
Provide Feedback