- Getting started
- Creating projects
- OPC UA
- Graphic objects
- Predefined graphic objects
- Sessions and locales
- Object and variable references
- Extending projects
- NetLogic
Create a thermometer linear gauge
Create a linear gage with a warning zone that indicates the current temperature.
- Create and configure the gauge:
- Right-clickMainWindow (Type)and select .
- Hover-over a gauge, select, and enterThermometerGauge.
- InProperties, create a dynamic link betweenValueand .For more information about dynamic links, see Create dynamic links.
- Set the value gauge warning zone:
- InProperties, next toWarning zones, select.
- UnderWarningZone1, setColorto#f30000.
- SetFromto75.
- SetToto100.
Provide Feedback