- Getting started
- Creating projects
- OPC UA
- Graphic objects
- Predefined graphic objects
- Sessions and locales
- Object and variable references
- Extending projects
- NetLogic
Create a dynamic alarm message
Create an alarm message that appears at runtime when the alarm is active. For example, create a message that indicates a flow rate or level is dangerously low when the alarm is active.
Prerequisites
- To create a dynamic alarm message
- InProject view, select the alarm.
- InProperties, inMessage, select, and then selectAdd Dynamic LinkAdvanced.
- In theDynamic Link Editor, inMessage, selectand then selectString formatter.
- InDynamic Link, select.Change Dynamic Link
- Specify theInput valueof the alarm as the source for the Dynamic Link.
- InFormat, enter the text of the alarm message, using the placeholder{0}to identify the value of the source variable.
- Select
as necessary to set the direction of the link.
Provide Feedback