- Getting started
- Creating projects
- OPC UA
- Graphic objects
- Predefined graphic objects
- Sessions and locales
- Object and variable references
- Extending projects
- NetLogic
Create a speed gauge and labels
Create UI elements that display speed-related information about a selected motor.
- Create the speed gauge:
- InProject view, right-clickMotorSpeedPaneland select .
- Hover-over the gauge, select, and enterSpeedGauge.
- InProperties, create a dynamic link betweenValueand .For more information about dynamic links, see Create dynamic links.
- Create the speed label:
- InProject view, right-clickMotorSpeedPaneland select .
- Hover-over the label, select, and enterSpeedLabel.
- InProperties, setTexttoSpeed.
- Create the speed value label:
- InProject view, right-clickMotorSpeedPaneland select .
- Hover-over the label, select, and enterSpeedValueLabel.
- InProperties, create a dynamic link betweenTextand .For more information about dynamic links, see Create dynamic links.
Provide Feedback