- Getting started
- Creating projects
- OPC UA
- Graphic objects
- Predefined graphic objects
- Sessions and locales
- Object and variable references
- Extending projects
- NetLogic
Add a Station Connection Status widget
Add a Station Connection Status widget to monitor the controller connection status.
Prerequisites
- To add a Station Connection Status widget
- From the main toolbar, select.Template Libraries
- InLibraries, search forStation Connection Status.
- UnderComponents, dragStation Connection StatustoMainWindow (type)or a different UI container inProject view.
- InProperties, create a dynamic link betweenStationand the communication driver station that you want to monitor.For more information about dynamic links, see Create dynamic links.
At runtime, the widget displays these LED status indicators:
- Green LED. Connected to the controller.
- Red LED. Disconnected from the controller.
Provide Feedback