Micro Controller Driver

Micro Controller Driver

Observe these guidelines when working with Micro Controller Driver.

Supported controllers

Micro Controller Driver supports
Micro800
controllers and
MicroLogix
1400 controllers.

Controller tags import

With Micro Controller Driver, you can import tags from
Micro800
controllers in the online mode.

Data types

Micro Controller Driver supports these data types:
Basic data types
Datatype
FactoryTalk Optix
datatype
BOOL
Boolean
SINT
SByte
DINT
Int32
REAL
Float
STRING
String
LREAL
Double
INT
Int16
LINT
Int64
USINT
Byte
BYTE
UINT
UInt16
WORD
UDINT
UInt32
DATE
TIME
DWORD
ULINT
UInt64
LWORD
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.