- Getting started
- Creating projects
- OPC UA
- Graphic objects
- Predefined graphic objects
- Sessions and locales
- Object and variable references
- Extending projects
- NetLogic
Set dynamic variables polling time for controllers
Set the time interval between readings of tag values from controllers at runtime.
- InProject view, selectNativePresentationEngineorWebPresentationEngine.For more information, see Presentation engines.
- InProperties, setDynamic variables polling time.TIP: Set the polling time between one sampling and the next in HHHH:MM:SS.MS format.
Provide Feedback