- Getting started
- Creating projects
- OPC UA
- Graphic objects
- Predefined graphic objects
- Sessions and locales
- Object and variable references
- Extending projects
- NetLogic
Create a dynamic link by selecting the source
Create a dynamic link using the
Properties
pane.- InProject view, select the node that contains the property to set through a dynamic link.
- InProperties, hover over the property value to set, and then select.Add Dynamic Link
- (optional) In the dynamic links browser, selectand selectConsistent Data Typeto make variables of incompatible types unavailable.For example, if the dynamic link parent expects a Boolean variable, all items except for Boolean variables will be grayed out in the dynamic links browser.
- Select a node to act as the source of the value property.
- Complete the displayed fields depending on the node selected:
- Attribute. Select the OPC UA attribute to apply to the selected node. For example, selectBrowseName,Value, orDisplayName.
- Format. Select the format to apply to the selected variable.
- Array index. Select the array index of the selected variable. This option appears for array variables only.
- Bit index. Select the index to access the specified bit of the selected variable.
- ChooseSelect.
The reference to the selected node or variable appears in the property. Before the property,
appears to indicate that the property contains a dynamic link.

TIP:
If the dynamic link does not resolve at design time,
appears before the dynamic link. A dynamic link to a Windows alias may resolve at runtime. If the dynamic link is broken because the linked attribute no longer exists or has been moved,
appears before the link.


Provide Feedback