- Getting started
- Creating projects
- OPC UA
- Graphic objects
- Predefined graphic objects
- Sessions and locales
- Object and variable references
- Extending projects
- NetLogic
Develop a gauge with a localized engineering unit
Create a linear gauge that displays the current temperature in a format adjusted to the logged in user.
Application example - Celsius degrees (it-IT)

Application example - Fahrenheit degrees (en-US)

NOTE:
Download a sample project:
LocalizedEngineeringUnitGauge.zipPrerequisites
- To develop the project
- Arrange the interface elements.
- Save the project.
Application design example

Select
to run the project using the client emulator to test your project. To run the project on a remote client, see Add a client device.
Run
Provide Feedback