- Getting started
- Creating projects
- OPC UA
- Graphic objects
- Predefined graphic objects
- Sessions and locales
- Object and variable references
- Extending projects
- NetLogic
Add an event to an object from another object
Add an event from an object to another object to avoid recreating the same event for multiple objects.
- InProject view, select the object to which you want to add the event.
- InPropertiesafterEvents, selectAdd external event.
- Navigate to the object that has the event you want to add to the current object, select the event, and then chooseSelect.
- To associate a method with the event, after the event, selectAdd net methodand select the desired method.
- In the selection window, navigate to and select the method and perform one of the following actions:
- To add aGlobal method, expand theCommandsnode and expand the method node to select a method.
- To add aLocal node, expand the node of the object to select a method.
- ChooseSelect.
- (optional) If the method requires arguments, expand the method and set the arguments.
Provide Feedback