- Getting started
- Creating projects
- OPC UA
- Graphic objects
- Predefined graphic objects
- Sessions and locales
- Object and variable references
- Extending projects
- NetLogic
FTP
File Transfer Protocol (FTP) is used to communicate and transfer files between computers that are on a Transmission Control Protocol/Internet Protocol (TCP/IP) network.
To establish and communicate on the network, an FTP connection requires a server and a client. The following section describes the configuration of these two elements.
Provide Feedback