- Getting started
- Creating projects
- OPC UA
- Graphic objects
- Predefined graphic objects
- Sessions and locales
- Object and variable references
- Extending projects
- NetLogic
Configure and FTP client
- Install stable versions of the following NuGet package: FluentFTP. See NuGet packages.
- Configure the requiredFTPClientLogicscript parameters. See FTP Client configuration.
- Run theFTPClientLogicscript.
Provide Feedback