- Getting started
- Creating projects
- OPC UA
- Graphic objects
- Predefined graphic objects
- Sessions and locales
- Object and variable references
- Extending projects
- NetLogic
Configure the editor grid
Configure the grid in the editor to show or hide the grid, align objects in the grid, and size the grid.
- InProject view, double-click a container object, or select.The editor opens in a new tab.
- In the editor toolbar, select.Grid settings
- Select the option to configure the grid:
- Grid Visible. Toggle showing the grid in the editor.
- Snap to grid. Align the edges of objects with the grid.
- Grid size. Specify the size of the grid in pixels.
Provide Feedback